EN
Choose your language

You would like to know the actual structure of metals and what is important in iron production?°

Here you can find out what materials actually are and why materials technology is important. You will learn step by step about the structure of metals, see how the combination of atoms forms the crystal lattice and how the structure is created from this. You will also learn which properties metals have. Finally, you will go through the process of extracting iron and producing steel and see what needs to be taken into account.

   

You will learn
What are materials and why is material technology important?

How are metals structured? Atoms - crystalline lattices - structure

What properties have metals?

How is pig iron won?

What should be considered in steel making? 
  

Materials history

Throughout history, we humans have needed materials for various everyday purposes. They have impacted different cultures and different eras have been named after them.

Werkstoffe historie

Material subdivisions

Materials can be split into metals or non-metals. Steel and cast iron are among the most commonly used materials worldwide.

Werkstoff Unterteilung

Materials technology and its importance

The purpose for which a particular material is used depends on its properties. These can be divided into different categories.

°°

Various scientific material technology methods are used to place materials into different categories and properties in the first place.

°°

Materials technology deals with extraction and use of materials and examines their various properties. This enables materials to be used properly, new materials to be developed and existing ones to be improved.

°°

Knowledge of the internal structure of materials is a prerequisite for analysing their properties. Only when you know what components a material is made up of and how these work are you able to gain new insights for further development.

Werkstofftechnik

Structure of metals

Aufbau von Metalle

Steel and cast iron possess many properties that make them among the most widely used materials in the world. When using them, we usually work with the finished product. But what is metal actually made up of?

°°

Many things are not visible to the naked eye. But with a microscope, you can see even the smallest components. 

Metals under the microscope

The positive charged particles of metal atoms are always arranged at fixed distances to one another, forming the crystalline lattice. They emit negative electrons, which surround the crystalline lattice as a so-called electron cloud. The electrons can move freely within this cloud, but cannot leave it.

The attraction of the positive and negative charges creates a strong metal bond. This ensures an extremely stable bond of the metal atoms and in turn the strength of the metal.

Summary of materials

You now know that materials have always played an important role and have characterised many eras and cultures. You have learnt that materials can generally be divided into metals and non-metals and can have different properties.°

You have also have learnt that materials technology is used to investigate the properties of materials so that new ones can be developed and existing ones improved. Finally, you have seen that metals are made up of a structure, crystal lattice and finally metal atoms, whose composition influences the metallic properties.

  

YOU HAVE°LEARNT°
Materials have always played an important role for humanity and have impacted many eras and cultures. 

Materials can be split into metals or non-metals. 

Material technology analyses the various properties of materials in order to develop new or improve existing materials. 

Metals are made up of a structure, crystalline lattice and metal atoms. 

These components influence metallic properties. 
 

Metals - structure and properties
How do metals conduct and how can they be deformed? 

What types of°crystal lattice°are there? 

Which°grid construction errors°can occur? 

How is a structure built? 

What are alloys and which types are there? 

What are status diagrams of alloys? 
 

  

Structure of metals

Now we will take a look at the exact structure of metals and their properties. To do this, you will first find out how metals conduct and can be deformed. You will get to know different types of crystalline lattice and see what kind of lattice defects can occur. Then we will take a closer look at the structure of metals and get to understand what happens with alloys. Finally, you will learn what types of alloys there are and how to read corresponding parametric diagrams.  

Conductivité des métaux

Metalle sind leifähig

Les métaux sont conducteurs et sont donc utilisés à diverses fins dans la vie quotidienne. La structure de leur réseau cristallin permet de mieux comprendre leur conductivité électrique.

Déformation des métaux

Outre leur conductivité électrique, les métaux sont également malléables. Ce faisant, ils subissent une déformation élastique ou plastique.

Revenons au niveau atomique dans le réseau cristallin. Lorsqu’une force est exercée sur une tôle, les atomes métalliques sont légèrement déplacés de leur position dans le réseau cristallin, mais ils reprennent ensuite leur place initiale. Cependant, dans le cas d’un bloc d’alliage, le déplacement dans le réseau cristallin persiste après la fin de l’application de la force, ce qui entraîne une déformation permanente.

Metalle sind verformbar

Réseaux cristallins des métaux

Vous savez déjà que les atomes métalliques ont un point commun : ils sont disposés en réseaux cristallins. Cependant, les réseaux cristallins ne se présentent pas toujours de la même manière. Selon le type de métal, la disposition géométrique des atomes dans le réseau cristallin varie également. 

   

Vous pouvez voir ici les trois principaux types de réseaux cristallins, avec leurs lignes de liaison. Celles-ci partent toujours du centre de l’atome et forment ainsi une disposition propre à chaque atome.

    Drei wichtigste Kristallgitterarten

    KUBISCH-RAUMZENTRIERT (KRZ) 

     KUBISCH-RAUMZENTRIERT (KRZ)

    Der Würfel besitzt ein Metallatom in der Mitte, das umschlossen wird. Da es nur locker gepackt ist, gibt es keine Stapelfolge. 

    Relativ viel Platz zwischen den Atomen ermöglicht Einlagerung zusätzlicher Fremdatome. 

        

    KUBISCH-FLÄCHENZENTRIERT (KFZ) 

    KUBISCH-FLÄCHENZENTRIERT (KFZ)

    Der Würfel besteht aus insgesamt 8 Atomen in den Würfelecken und je einem Atom in der Mitte der Seitenflächen. 

    Die Atome sind in drei Stapeln angeordnet (ABC) und bilden dadurch eine dichteste Kugelpackung. 

    Eine gestörte Stapelfolge führt zu Stapelfehlern, in die Legierungselemente eingelagert werden können. Daraus ergeben sich andere Eigenschaften. 


       

    HEXAGONAL-DICHTEST GEPACKT (HDR) 

    HEXAGONAL-DICHTEST GEPACKT (HDR)

    Die Metallatome sind in einem sechseckigen Prisma angeordnet mit je einem Atom in der Mitte der Grundflächen. 3 Atome befinden sich innerhalb des Prismas. 

    Die Stapelfolge ist ABA und bildet so eine dichteste Kugelpackung. 

    Große Gitterlücken bieten Platz für Fremdatome. 

    Schlechter kalt umformbar als Metalle mit kfz-Gitter. 

    Gitterbaufehler

    Metalle sind keine Idealkristalle, sondern weisen Gitterfehler auf. Je nach Art und Größe lassen sich die Gitterfehler drei Dimensionen zuordnen. Die erste Dimension sind die nulldimensionalen Fehler. Diese entsprechen einem Gitterpunkt und lassen sich nochmals unterteilen.

    Die nulldimensionalen Fehler haben in der Regel keine negativen Auswirkungen auf Eigenschaften metallischer Werkstoffe, sondern ermöglichen sogar wichtige Wärmebehandlungen.

    Eindimensionalen Fehler

    Daneben gibt es noch die eindimensionalen Fehler, auch Linienfehler genannt. Wird eine Halbebene in das reguläre Kristallgitter eingeschoben, ist die Linie gestört und es bildet sich so eine Stufenversetzung. Versetzungen sind beweglich und somit Ursache für die plastische Verformbarkeit von Metallen.

    eindimensionalen Fehler

    zweidimensionalen Fehlern

    zweidimensionalen Fehlern 

    Bei zweidimensionalen Fehlern kommt es zu Stapelfehlern     der regulären Schichtenfolge. Stapelfehler entstehen durch   Kristallisation oder durch Zusammenfallen eines   Leerstellenclusters. Zweidimensionale Gitterfehler haben   Einfluss auf die Zugfestigkeit eines Metalls. 

    Gefüge

    Sie haben bereits erfahren, dass Metalle aus vielen regelmäßig geformten Körnern bestehen, die in ihrer Vielzahl das Gefüge bilden. Mit bloßem Auge ist das Gefüge nicht zu erkennen. Doch mit einem metallografischen Schliffbild kann das Gefüge unter einem Metallmikroskop sichtbar gemacht werden. 

    Das Schliffbild zeigt die Korngröße und die Korngrenzen eines Metalls. Die Korngröße reicht von feinkörnig bis grobkörnig und lässt sich durch gezielte Behandlung einstellen. Korngrenzen stellen Unterbrechungen der Atomanordnung der Körner dar und zählen zu den erwähnten zweidimensionalen Gitterfehlern. Diese entstehen beispielsweise während der Kristallisation. 

    Gefüge

    Feinkörnige Metalle haben bessere mechanische Eigenschaften gegenüber grobkörnigen, da es mehr Korngrenzen gibt. Eine Erhöhung der Korngrenze verbessert die Zähigkeit.  Allerdings entstehen bei erhöhten Temperaturen unerwünschte Kriechvorgänge.

    Kornformen

    Neben der Gemeinsamkeit von Korngröße und Korngrenzen gibt es je nach Metall und Kristallgittertyp unterschiedliche Kornformen.

    GLOBULARE KÖRNERGLOBULARE KÖRNER

    Rundliche Körner, z. B. reines Eisen 

    POLYEDRISCHE KÖRNER POLYEDRISCHE KÖRNER

    Körner in Vieleckform, z. B. Eisen mit Austenitgefüge

    DENDRITISCHE KÖRNER DENDRITISCHE KÖRNERNadelartige Körner, z. B. gehärteter Stahl 

    LAMELLENARTIGE GEFÜGE LAMELLENARTIGE GEFÜGELamellenartig geformte Kristalle, z. B. Lamellengrafit von Grauguss 

    Legierungen

    Sie haben bereits erfahren, dass Metalle keine Idealkristalle sind, sondern beabsichtigte Gitterbaufehler aufweisen. Aus all den Metallen im Periodensystem kommt nur das Edelmetall 'Gold' in reiner Form vor. Alle weiteren metallischen Werkstoffe sind Metallgemische und nennen sich Legierungen.

    Im Legierungsvorgang werden ein oder mehrere metallische Elemente absichtlich in das Kristallgitter eines Metalls eingefügt, um gewünschte Eigenschaftsänderungen zu erzielen.

    Legierungen

    Legierungsvorgang

    Wird nach dem Legierungsvorgang die Temperatur wieder gesenkt, beginnt die Schmelze abzukühlen und bildet beim Erstarren mit dem Legierungselement ein neues Metallgemisch.

    Arten von Legierungen

    Die Legierungselemente können sich auf unterschiedliche Weise in das Grundmetall einlagern und bilden im festen Zustand zwei unterschiedliche Gefügearten.

    Mischkristall-Legierung

    Mischkristall-Legierung

    Kristallgemisch-Legierung

    Kristallgemisch-Legierung

    Mischkristall-Legierungen sind im flüssigen Zustand vollständig ineinander löslich. Beim Erstarren verteilen sich die Metalle gleichmäßig. Sie sind fester als reine Grundmetalle, dabei aber gut umformbar. Kristallgemische sind ebenfalls im flüssigen Zustand ineinander löslich, im festen Zustand lagern sich die Metalle dann getrennt zusammen.

    Zustandsdiagramme von Legierungen

    Zur Erforschung und Weiterentwicklung der Eigenschaften von Legierungen werden deren Zustandsdiagramme analysiert. Allgemein bilden Zustandsdiagramme die Aggregatzustände reiner Metalle ab. Dafür wird der Knickpunkt in der Abkühlungs- beziehungsweise Erwärmungskurve verwendet. 

    Zustandsdiagramme von Legierungen

    Bei Legierungen kommt noch die Temperatur des zweiten Metalls hinzu sowie das Mischungsverhältnis in der Legierung. Werden nun alle Knickpunkte übertragen und die Temperaturpunkte verbunden, ergibt sich das Zustandsdiagramm für die Legierung.   

    Mischkristalle und Kristallgemische haben unterschiedliche Zustandsdiagramme. Mischkristalle wie Kupfer und Nickel sind geprägt durch eine vollständige Löslichkeit im flüssigen und festen Zustand.

       

    Zustandsdiagramme von Kristallgemische

    Das Zustandsdiagramm für Kristallgemische wie Blei und Zinn sieht anders aus. Dieses ist durch eine vollständige Löslichkeit im flüssigen und Unlöslichkeit im festen Zustand geprägt.

       

    SIE HABEN ERFAHREN 
    Elektrischer Strom ist der Fluss von Elektronen.

    Metalle lassen sich elastisch (reversibel) oder plastisch (irreversibel) verformen.

    Die drei wichtigsten Kristallgitterarten sind: Kubisch-flächenzentriert (kfz), Kubisch-raumzentriert (krz), Hexagonal-dichtest gepackt (hdp)

    Metalle sind keine Idealkristalle, sondern weisen Gitterfehler auf: Nulldimensionale Fehler, Eindimensionale Fehler, Zweidimensionale Fehler

    Das Gefüge besteht aus einer Vielzahl regelmäßig geformter Körner.

    Bei Legierungen werden metallische Elemente absichtlich in das Kristallgitter eingefügt. Dadurch entstehen Mischkristalle und Kristallgemische.

    Zustandsdiagramme bilden die Aggregatzustände von Legierungen ab. 

    L’extraction de la fonte brute

    Dans la dernière partie, nous allons d’abord voir comment on extrait la fonte brute et quelles sont les étapes importantes de ce processus. Vous découvrirez ensuite les différents procédés permettant de transformer la fonte brute en acier. Pour finir, vous verrez les différentes méthodes de traitement ultérieur et de coulée de l’acier. 

    Comme vous l’avez appris, l’acier est l’un des matériaux les plus utilisés au monde. Son principal composant est le fer. Le fer est présent dans la nature sous forme de minerai de fer, un composé de fer et d’oxygène. Pour fabriquer de l’acier, le fer doit d’abord être extrait au moyen de procédés de réduction. 

    Deux procédés de réduction sont utilisés pour l’extraction de la fonte brute. Voici un aperçu de ces deux procédés. 

    Gewinnung von Roheisen

    La fabrication de l’acier

    Une fois la fonte brute, ou l’éponge de fer solide, obtenue, on passe à ce que l’on appelle les « procédés d’affinage » pour produire l’acier. Pouvez-vous imaginer ce qui se passe lors de l’affinage ? 

    Dans le procédé de soufflage à l’oxygène, la fonte brute liquide est versée dans un convertisseur avec de la ferraille et des additifs. Un tube refroidi à l’eau insuffle de l’oxygène dans ce récipient, ce qui provoque une réaction chimique avec les particules de fer. Le carbone contenu dans la fonte brute s’oxyde et la chaux vient fixer les impuretés présentes dans le fer. L’acier et les scories sont ensuite coulés.

     Sauerstoffaufblas-Verfahren

    Le procédé du four à arc électrique est utilisé pour la fabrication d’aciers fortement alliés. Pour ce faire, on remplit une cuve de fusion de fonte brute et d’autres composants. On place des électrodes en carbone par-dessus, puis on déclenche un arc électrique. Le carbone résiduel et les impuretés sont éliminés par combustion au cours de la fusion. L’acier et les scories sont ensuite coulés.

    Elektrolichtbogenofen-Verfahren

    Après la fabrication de l’acier, il reste souvent des composants indésirables. Pour obtenir des aciers de qualité, on élimine ces composants en recourant à des traitements ultérieurs. Vous trouverez ici les principaux procédés et leur description. Sélectionnez les procédés pour en savoir plus. 

    Trattamento secondario e colata

    DISOSSIDAZIONE 
    Gli elementi disossidanti legano l'ossigeno che si libera durante la solidificazione del metallo fuso. 
    In questo modo si evita la formazione di cavità contenenti aria o gas. 
    DESOXIDATION

    Degassaggio sotto vuoto

    Il travaso dell'acciaio liquido favorisce la fuoriuscita dei gas residui. 
    Altrimenti tali gas possono causare tensioni interne e piccole cricche nell'acciaio.

    Vakuum-Entgasung

    Processo di rifusione

    Il blocco di acciaio inox viene inserito in uno stampo di acciaio (lingottiera) come elettrodo. Un arco elettrico fonde il blocco di acciaio in un bagno di scorie. 
    L'acciaio fuso gocciola attraverso le scorie di affinazione che legano le ultime impurità.

    Umschmelz-verfahren

    Trattamento con gas di spurgo

    Il gas di spurgo trascina le varie impurità verso la superficie.

    Spülgasbehandlung

      

    Una volta completato il trattamento secondario, l'acciaio fuso viene colato e assume così la forma iniziale per la successiva fase di lavorazione. A tal fine vengono utilizzati due procedimenti. Nella colata continua, l'acciaio scorre in continuo in una lingottiera raffreddata ad acqua. Al termine del processo si ottiene un semiprodotto che deve poi essere laminato.

    Strangguss Verfahren

       

    Per lingotti di acciaio di grandi dimensioni si impiega la colata in lingottiere apposite. In questo processo l'acciaio fuso viene colato in stampi di acciaio. Dopo la solidificazione, gli stampi vengono sfilati quando sono ancora a temperatura di incandescenza. Una volta raffreddati, i blocchi di acciaio possono essere utilizzati come pezzi da fucinare o come semilavorati da laminare. 

       

    Kokillen-Blockguss Verfahren

       

    Riepilogo

    Sapete ora che il ferro deve essere prima estratto dal minerale di ferro e che ciò avviene in un altoforno o per riduzione diretta. Avete anche appreso che nella produzione dell'acciaio vengono utilizzati diversi processi di affinazione per ridurre il contenuto di carbonio ed eliminare le impurità. 

    Infine, avete approfondito i diversi processi di trattamento dell'acciaio. Questi vengono utilizzati per eliminare eventuali residui indesiderati ancora presenti. Conoscete ora anche i due procedimenti di colata che preparano l'acciaio per le successive lavorazioni. 

       

    NOZIONI ACQUISITE 
    Il ferro viene estratto dal minerale ferroso (tramite altoforno o riduzione diretta). 

    I processi di affinazione sono utilizzati per ridurre il tenore residuo di carbonio ed eliminare le impurità.

    Il trattamento secondario dell'acciaio serve per eliminare i residui di componenti indesiderati.

    La colata dell'acciaio serve a preparare l'acciaio per le successive lavorazioni.